Skip to main content
mahmoud boroumand
Associate III
Feb 12, 2018 1:26 PM UTC
Question

change open drain to pp

Posted on February 12, 2018 at 14:26

hello 

i use this configuration for send for ws2812.

GPIO_InitStructure.GPIO_Pin = WS2812B_PINS;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_OD;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(WS2812B_PORT, &GPIO_InitStructure);

I because i need 5v i use this configuration (use 2.2K for pull up). but i now i want chage port to pp and 3.3 v and do this configuration 

GPIO_InitStructure.GPIO_Pin = WS2812B_PINS;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(WS2812B_PORT, &GPIO_InitStructure);

but i have a problem if the mcu use to open drain if i change to pp i have noise on it but if it is new i don't have any problem what can i  do?

    This topic has been closed for replies.

    3 replies

    T J
    Senior III
    Feb 12, 2018 1:42 PM UTC
    Posted on February 12, 2018 at 14:42

    are you discussing the serial LED driver ?

    its likely to work with 3V data in,. did you try it ?

    you can use a transistor or FET to translate the voltage, but some configurations invert the data, some don't.

    easiest is:  2 resistors, 1 npn transistor but returns an inverted output.

    AvaTar
    Senior III
    Feb 12, 2018 1:55 PM UTC
    Posted on February 12, 2018 at 14:55

    but i have a problem if the mcu use to open drain if i change to pp i have noise on it but if it is new i don't have any problem what can i  do?

    If I understand this convoluted and careless punctuated sentence correctly:  Have you tried a proper de-init of the pin ?

    Un-set the old pin configuration first, then set the new one.

    ... if i change to pp i have noise on it...

    This suggests you did not really change to PP, I view 'noise' as symptom of OD without a load resistor.

    Andrew Neil
    Super User
    Feb 12, 2018 2:37 PM UTC
    Posted on February 12, 2018 at 15:37

    if i change to pp i have noise on it

    on what, exactly?

    And what sort of 'noise', exactly, is it?

    Post a proper schematic of your two setups, and oscilloscope traces of the signals.

    Instead of changing to PP, what happens if you just set PP from the outset ... ?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.