Skip to main content
NASI
Associate III
October 4, 2021
Solved

Challeng with I2C1 and I2C2

Hello,

I am working with a costumer board using STM32F105. There are some LED drivers working I2C1 and I2c2.

Configuration for serial interfaces is:

void MX_I2C1_Init(void)

{

 /* USER CODE BEGIN I2C1_Init 0 */

 /* USER CODE END I2C1_Init 0 */

 /* USER CODE BEGIN I2C1_Init 1 */

 /* USER CODE END I2C1_Init 1 */

 hi2c1.Instance = I2C1;

 hi2c1.Init.ClockSpeed = 100000;

 hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;

 hi2c1.Init.OwnAddress1 = 0;

 hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;

 hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;

 hi2c1.Init.OwnAddress2 = 0;

 hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;

 hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;

 if (HAL_I2C_Init(&hi2c1) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN I2C1_Init 2 */

 /* USER CODE END I2C1_Init 2 */

}

/* I2C2 init function */

void MX_I2C2_Init(void)

{

 /* USER CODE BEGIN I2C2_Init 0 */

 /* USER CODE END I2C2_Init 0 */

 /* USER CODE BEGIN I2C2_Init 1 */

 /* USER CODE END I2C2_Init 1 */

 hi2c2.Instance = I2C2;

 hi2c2.Init.ClockSpeed = 100000;

 hi2c2.Init.DutyCycle = I2C_DUTYCYCLE_2;

 hi2c2.Init.OwnAddress1 = 0;

 hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;

 hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;

 hi2c2.Init.OwnAddress2 = 0;

 hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;

 hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;

 if (HAL_I2C_Init(&hi2c2) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN I2C2_Init 2 */

 /* USER CODE END I2C2_Init 2 */

}

HW connections should be correct, because I am able to turn all LEDs which they configured in I2C1 and I2C2. But after some tries, I miss I2C1 and ErrorCode 32 (Timeout error) show up.

For I2C1, the errorcode is 32, and for I2C2 there is no error.

I am using 10ms for timeout for both I2C's, and it doesn't help if I put more timeout.

I am using following function to write the value on serial interface with related data:

void WriteRegister(HandleTypeDef* handle, uint8_t register_address, uint8_t value)

{

uint8_t buf[2];

buf[0] = register_address;

buf[1] = value;

HAL_I2C_Master_Transmit(handle->Init.I2C_Bus, handle->Init.I2C_Device_Address, buf, 2, handle->Init.I2C_Transmit_Timeout_Milliseconds);

}

Any idea?

Thank you.

This topic has been closed for replies.
NASI
NASIBest answer
Associate III
October 13, 2021

Thank you @TDK​ and @Amel NASRI​ .

Some HW issues have been found for the LED drivers circuit. It seems to be work fine now. I need to test with other prototypes as well.

4 replies

TDK
October 4, 2021

Sounds like a hardware issue.

Which line within HAL_I2C_Master_Transmit produces the timeout?

Do you have a logic analyzer to show the SDA/SCL lines?

Are there pullups on both lines?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Amel NASRI
ST Technical Moderator
October 13, 2021

Hi @NASI​ ,

Besides to proposals from @TDK​ , I suggest you to have a look to the product errata sheet.

Several known limitations on the I2C of STM32F1 are described on this document.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
NASI
NASIAuthorBest answer
Associate III
October 13, 2021

Thank you @TDK​ and @Amel NASRI​ .

Some HW issues have been found for the LED drivers circuit. It seems to be work fine now. I need to test with other prototypes as well.

Amel NASRI
ST Technical Moderator
October 13, 2021

Good to know that you identified the root cause of your issue.

I mark your reply as best answer. In case you have new questions, don't hesitate to create new inputs.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.