Skip to main content
john doe
Senior III
August 9, 2017
Question

Chaining 16 bit timers to a 32 bit timer. Am I understanding it?

  • August 9, 2017
  • 1 reply
  • 761 views
Posted on August 09, 2017 at 04:18

Might as well learn something as long as the cubemx app isnt getting it right

I get stumped by the terminology sometimes because it tends to vary in the documentation.

In order to chain together two 16-bit timers into one 32 bit timer, I need to:

set up the first timer as oc output one pulse mode

do I want the slave in reset mode or gated mode?

    This topic has been closed for replies.

    1 reply

    Tomas DRESLER
    Associate II
    August 9, 2017
    Posted on August 09, 2017 at 10:39

    First timer free running, with master output on update event (i.e. reset of the counter)

    Second timer as slave External clock mode with proper ITRx input