Question
Capture input PWM analog signal using Timers.
I have a specific requirement to capture input PWM analog signal using Timers.
The timer should capture both period and duty cycle of the input signal for one pulse, then stop the capture automatically.
The application can read the capture compare register (CCR1, CCR2) and enable the capture again.
MCU : STM32F207
I read the reference manual of the STM32F207 mcu (page 395, section 14.3.6 PWM input mode). I did not find a way to configure the timer for the above requirement.
Can someone please enlighten me with specific configuration ?