cant get x or y values on XPT2046 over SPI on STM32F407VE
I just got https://stm32-base.org/boards/STM32F407VET6-STM32-F4VE-V2.0 which is my first foray into embeded. I also got https://www.waveshare.com/wiki/4inch_Resistive_Touch_LCD which is TFT with XPT2046 touch. I have the LCD setup with FSMC 16-bit but I can't get touch working.
static void MX_SPI2_Init(void)
{
/* USER CODE BEGIN SPI2_Init 0 */
/* USER CODE END SPI2_Init 0 */
LL_SPI_InitTypeDef SPI_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Peripheral clock enable */
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_SPI2);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOB);
/**SPI2 GPIO Configuration
PB13 ------> SPI2_SCK
PB14 ------> SPI2_MISO
PB15 ------> SPI2_MOSI
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_13|LL_GPIO_PIN_15;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_14;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* USER CODE BEGIN SPI2_Init 1 */
/* USER CODE END SPI2_Init 1 */
/* SPI2 parameter configuration*/
SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX;
SPI_InitStruct.Mode = LL_SPI_MODE_MASTER;
SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT;
SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_LOW;
SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE;
SPI_InitStruct.NSS = LL_SPI_NSS_SOFT;
SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV256;
SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
SPI_InitStruct.CRCPoly = 10;
LL_SPI_Init(SPI2, &SPI_InitStruct);
LL_SPI_SetStandard(SPI2, LL_SPI_PROTOCOL_MOTOROLA);
/* USER CODE BEGIN SPI2_Init 2 */
/* USER CODE END SPI2_Init 2 */
}SPI code
static void MX_GPIO_Init(void)
{
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOH);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOC);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOB);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOE);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOD);
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_GPIOA);
/**/
LL_GPIO_SetOutputPin(LCD_RST_GPIO_Port, LCD_RST_Pin);
/**/
LL_GPIO_SetOutputPin(GPIOB, BL_Pin|TP_CS_Pin);
/**/
GPIO_InitStruct.Pin = LCD_RST_Pin;
GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
LL_GPIO_Init(LCD_RST_GPIO_Port, &GPIO_InitStruct);
/**/
GPIO_InitStruct.Pin = TP_IRQ_Pin;
GPIO_InitStruct.Mode = LL_GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
LL_GPIO_Init(TP_IRQ_GPIO_Port, &GPIO_InitStruct);
/**/
GPIO_InitStruct.Pin = BL_Pin;
GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_UP;
LL_GPIO_Init(BL_GPIO_Port, &GPIO_InitStruct);
/**/
GPIO_InitStruct.Pin = TP_CS_Pin;
GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(TP_CS_GPIO_Port, &GPIO_InitStruct);
}GPIO code
#define Y 0x90 //9C //94 //90
#define X 0xD0 //DC //D4 //D0
#define CS_TOUCH_SELECT() LL_GPIO_ResetOutputPin(TP_CS_GPIO_Port, TP_CS_Pin)
#define CS_TOUCH_DESELECT() LL_GPIO_SetOutputPin(TP_CS_GPIO_Port, TP_CS_Pin)
uint32_t XPT2046_irq_read(void)
{
return LL_GPIO_IsInputPinSet(TP_IRQ_GPIO_Port, TP_IRQ_Pin);
}
static uint8_t SendReceive_Data8(SPI_TypeDef *SPIx, uint8_t data)
{
while(!LL_SPI_IsActiveFlag_TXE(SPIx)) {}
LL_SPI_TransmitData8 (SPIx, data);
while(!LL_SPI_IsActiveFlag_RXNE(SPIx)) {}
//(void) SPIx->DR; //fake Rx read;
while (LL_SPI_IsActiveFlag_BSY(SPIx));
return LL_SPI_ReceiveData8(SPIx);
}
void XPT2046_init(void)
{
CS_TOUCH_SELECT();
SendReceive_Data8(SPI2, 0X80);
SendReceive_Data8(SPI2, 0X00);
SendReceive_Data8(SPI2, 0X00);
LL_mDelay(5);
CS_TOUCH_DESELECT();
}XPT2046 library by https://github.com/ScarsFun/lvgl_STM32F103_ILI9341_XPT2046
when i touch screen it registers touch, so IRQ is working. in the SendReceive_Data8 function, it gets stuck on the first two while loops. if i comment them out and add a delay, it just returns 0. maybe i setup SPI wrong or its not initializing? all the examples of XPT2046 i found seem to do the same init so i guess its my SPI config
id appreciate any help! thanks