Skip to main content
jpeacock2399
Associate III
June 20, 2012
Question

Cannot set EXTICR register in STM32F205

  • June 20, 2012
  • 14 replies
  • 3351 views
Posted on June 21, 2012 at 00:14

Following the example for the STM3240G I set up the KEY pushbutton (PG15) as an external interrupt:

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG, ENABLE); // enable port 
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); // enable external interrupts 
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOG, EXTI_PinSource15); // KEY switch IRQ 
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; // inputs 
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; // external pull-ups 
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; // slow inputs 
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15; 
GPIO_Init(GPIOG, &GPIO_InitStructure); // PG15 KEY pushbutton 
// Enable the EXTI line 15 on falling edge for KEY pushbutton 
EXTI_ClearITPendingBit(EXTI_Line15); // clear pending IRQs 
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; 
EXTI_InitStructure.EXTI_Line = EXTI_Line15; // set up irq trigger 
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling; // falling edge on button push 
EXTI_InitStructure.EXTI_LineCmd = ENABLE; 
EXTI_Init(&EXTI_InitStructure); 
NVIC_InitStructure.NVIC_IRQChannel = EXTI15_10_IRQn; // KEY irq vector (shared) 
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = GPIODEV_EXT_PRIORITY; 
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; 
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; 
NVIC_Init(&NVIC_InitStructure);

I verified the SYSCFG is enabled, RCC_APB2ENR is set to 0x4000 (SYSCFG clock on). However, after I do the

SYSCFG_EXTILineConfig

call the SYSCFG->EXTICR4 register is still set to 0x0000. Pin PG15 is not linked to EXTI No interrupt occurs. Is there some setting which holds SYSCFG in reset? The obvious suspect is the SYSCFG peripheral clock but it shows as enabled. The PG15 pin itself is working. The pushbutton shows up in the GPIOG->IDR register, so the problem seems to be the SYSCFG EXTICRn registers. I tried directly writing to the EXTICR4 register (0x6000, G15) but it reads back as zero. Jack Peacock #syscfg-exti
This topic has been closed for replies.

14 replies

bart239955_st
Associate
October 30, 2012
Posted on October 30, 2012 at 11:38

Did you guys sorted out what was the problem meanwhile?

It seems I'm experiencing exactly the same problem. I compared my code to the above listings several times now and I can't find any mistakes.

Tesla DeLorean
Guru
October 30, 2012
Posted on October 30, 2012 at 14:56

I haven't dwelt on it since.

If it's not the software, examine the hardware. Look at some of the STM322xG-EVAL examples.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
bart239955_st
Associate
October 30, 2012
Posted on October 30, 2012 at 17:21

It was the software after all of course …

I’m working on a STM3220G evaluation board so the chances that anything was wrong there were pretty low.

The plan was to have an interrupt on pressing the key listed ‘key’ on the silkscreen of the evaluation board. (B4) – This key is connected to port PG15.

It seems I then managed to look at the wrong bit in the interrupt pending register of the NVIC.

PG15 can be connected to EXTI12 till EXTI15.

EXTI lines 10 till 15 have their own vector in the vector table and I managed to overlook that. (Waiting for the IRQ arriving on EXTI4 … and being surprised that nothing happens!)

Now that I found out how it work this looks pretty silly I know.

                /* Enable and set EXTI Line10-15 Interrupt to the lowest priority */

                NVIC_InitStructure.NVIC_IRQChannel =

EXTI15_10_IRQn

;

                 

                NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0F;

                NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x0F;

                NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

                NVIC_Init(&NVIC_InitStructure);

Tesla DeLorean
Guru
October 30, 2012
Posted on October 30, 2012 at 18:15

That's certainly an easy thing to do, one of my big gripes with the library is the lack of numeric parameters, so general/adaptable solutions are difficult.

Change a DMA stream and you have to resolve a dozen references, catching them all.

Thing2, SomethingElse2, SimilarButDifferent2, ... which all have enumerations other than TWO.

I understand the implementation efficiency of using bit vectors and masks, but it becomes a bugger to retarget a peripheral, or use two without duplicating code.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..