Question
Cannot for the life of me get TIM2 to trigger ADC1
Posted on April 03, 2012 at 08:00
Hi all,
Bit at my wits end here. I have been trying for quite some time to get ADC1 to trigger on TIM2 CC2. To start with, I tried to use TIM3 TRGO with about the same amount of luck (ie none). Everything works fine if I put ADC->CR2 = ADC_CR2_ADON in the timer interrupt, so that I have at least done something right. The DAC is just in there so I can see the counter value on my oscilloscope. Does anyone have any idea what on earth I am doing wrong? Any help at all would be very much appreciated! I am using an STM32VLDiscovery (STM32F100) with GCC.
#define CPU_SPEED 24000000
#include ''stm32f10x.h''
void
TIM2_IRQHandler(
void
) {
if
(TIM2->SR & TIM_SR_UIF) {
TIM2->SR &= ~TIM_SR_UIF;
}
if
(TIM2->SR & TIM_SR_CC2IF) {
TIM2->SR &= ~TIM_SR_CC2IF;
GPIOC->ODR |= (1<<9);
}
}
void
adc1_init() {
RCC->APB2ENR |= RCC_APB2ENR_ADC1EN;
// clock on
ADC1->CR1 = ADC_CR1_EOCIE;
// eoc interrupt, channel 0
ADC1->CR2 = ADC_CR2_EXTTRIG | ADC_CR2_EXTSEL_1 | ADC_CR2_EXTSEL_0;
// external trigger, tim2 cc2 trigger
ADC1->CR2 = ADC_CR2_ADON;
// wake up ADC (needs to be done with its own write)
NVIC->ISER[0] |= (1 << (ADC1_IRQn & 0x1F));
// IRQ enable
}
void
ADC1_IRQHandler(
void
) {
if
(ADC1->SR & ADC_SR_EOC) {
ADC1->SR &= ~ADC_SR_EOC;
GPIOB->ODR = ADC1->DR;
}
}
int
main(
void
)
{
int
j = 0;
RCC->APB2ENR |= RCC_APB2ENR_IOPAEN | RCC_APB2ENR_IOPBEN | RCC_APB2ENR_IOPCEN;
adc1_init();
// configure portc lower to be output
GPIOC->CRL = 0x11111111;
// all general purpose push-pull output
GPIOC->CRH = 0x11111111;
GPIOC->ODR = 0x00000000;
GPIOB->CRL = 0x11111111;
GPIOB->CRH = 0x11111111;
// GPIOB too!
// enable tim2 (general purpose timer)
RCC->APB1ENR |= RCC_APB1ENR_TIM2EN;
NVIC->ISER[0] |= (1 << (TIM2_IRQn & 0x1F));
// enable position 28 interrupt (TIM2)
TIM2->PSC = 0xFFFF;
// huge prescaler
TIM2->DIER = TIM_DIER_UIE | TIM_DIER_CC2IE;
// compare 2 interrupt enable
TIM2->ARR = 0xF;
// count up to 0xF
TIM2->CCR2 = 0x6;
// trigger at 0x6
TIM2->CR1 = TIM_CR1_CEN;
// enable the clock
TIM2->EGR = 1;
// update the shadow registers
// init dac
RCC->APB2ENR |= RCC_APB2ENR_IOPAEN;
GPIOA->CRL = 0;
RCC->APB1ENR |= RCC_APB1ENR_DACEN;
DAC->CR |= DAC_CR_EN1;
while
(1) {
if
(TIM2->CNT != 0x6) GPIOC->ODR &= ~(1<<9);
DAC->DHR12R1 = TIM2->CNT*256;
// output the counter value
}
}