Skip to main content
b.a.
Associate III
Dec 11, 2024 11:08 AM UTC
Question

cannot connect with GDB/openOCD but no problem with STM32CubeProgrammer

I have a strange problem

 

I use sloeber, an eclipse arduino "plugin" and up to now that worked fine.

Now I wanted to debug a custom STM32L412KB board and I can't connect to the MCU.

I always get an error message that the MCU cannot be found

 

 

 

xPack Open On-Chip Debugger 0.12.0+dev-01557-gdd1758272-dirty (2024-04-02-07:27)
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "hla_swd". To override use 'transport select <transport>'.
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
Started by GNU MCU Eclipse
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 500 kHz
Info : STLINK V2J43M28 (API v2) VID:PID 0483:374B
Info : Target voltage: 3.242904
Error: init mode failed (unable to connect to the target)

 

 

 

 

the debugger is a STM32L4R5 eval board

but connecting/erasing/flashing with STM32CubeProgrammer works fine with the very same setup

 

I use the same SW stack to debug custom STM32L4R5 boards, but this time with a STLINK-V3MINIE
I am not familiar with GDB/openOCD, up to now it just worked almost out of the box

 

any hint appreciated!

This topic has been closed for replies.

1 reply

ST Technical Moderator
Dec 20, 2024 12:13 PM UTC

Hello @b.a. 

Make sure to upgrade your firmware and use latest release of STM32CubeProgrammer.

Check your connectivity pins and jumper on the board and try  "Connect Under Reset" mode.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks