Skip to main content
juriedutoit
Associate
July 6, 2016
Question

Cannot change system speed for STM32F746IG

  • July 6, 2016
  • 1 reply
  • 545 views
Posted on July 06, 2016 at 08:42

I designed a PCB and I am programming the STM32F746IG via a FT2232D chip.  I have the 4 x JTAG signals connected to the STM32.

I generate code with MXCube, it compiles, but when I run it, Crossworks goes into an enless loop giving me gives me ''Stopped by Vector Catch''.  I have pin pointed it to the function : main.c -> SystemClock_Config(void) -> ''if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)'' -> ''__HAL_RCC_PLL_ENABLE();'' (just after the call to ''WRITE_REG(...)'')

I also used MXCube to generate a Keil MDK V5 project, it compiled, but the same happened in the Keil development environment.

How do one change the clock frequency of the PLL to 216MHz?

Please advise!

Thanks
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    July 6, 2016
    Posted on July 06, 2016 at 15:29

    [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/Cannot%20change%20system%20speed%20for%20STM32F746IG&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx&currentviews=7]cross posted

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..