Skip to main content
NSood.1
Visitor II
February 21, 2020
Question

CAN2 peripheral configuration

  • February 21, 2020
  • 0 replies
  • 492 views

I have this code attached which is configured to run both CAN1 and CAN2 peripherals however the TX functionality which is what I was trying to use is working on CAN1 but not on CAN2 (trying to send a packet using ADDmessage TX routine), I double checked with another sniffer hardware and CAN1 works.

However, I'm configuring the CAN2 with exactly the same parameters as that of the CAN1, is it right or does CAN 2 have to have different settings!?

System is STM32F429 discovery board with SN65HVD230 transceiver.

This topic has been closed for replies.