Skip to main content
jps2
Associate
March 29, 2010
Question

CAN2 in STM32F105

  • March 29, 2010
  • 4 replies
  • 1009 views
Posted on March 29, 2010 at 22:17

CAN2 in STM32F105

    This topic has been closed for replies.

    4 replies

    jps2
    jps2Author
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:45

    Thank you michi.

    I can transmit data so I use the CAN 1 clock.

    My problem is that I can't receive data?

    Any Idea?

    Ragards

    JeePee

    michi
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:45

    You must activate clock for CAN1 to send with CAN2.

    michi
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:45

    I had the same problem with the STM23F107 with CAN2.

    You must activate clock for CAN1 and CAN2 and set the filter for CAN2:

    /* CAN1 Periph clock enable */

      RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);

      /* CAN2 Periph clock enable */

      RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN2, ENABLE);

    Filter settings for example for all IDs

    /**

      * @brief  Configures the CAN2 filter.

      * @param  None

      * @retval None

      */

    void CAN2_Filter_Config_None(void)

    {

      CAN_FilterInitTypeDef   CAN_FilterInitStructure;

     

      /* CAN filter init */

      CAN_FilterInitStructure.CAN_FilterNumber=14; // for CAN2 begins the filter number with number 14

      CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdMask;

      CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_32bit;

      CAN_FilterInitStructure.CAN_FilterIdHigh=0x0000;

      CAN_FilterInitStructure.CAN_FilterIdLow=0x0000;

      CAN_FilterInitStructure.CAN_FilterMaskIdHigh=0x0000;

      CAN_FilterInitStructure.CAN_FilterMaskIdLow=0x0000;

      CAN_FilterInitStructure.CAN_FilterFIFOAssignment=0;

      CAN_FilterInitStructure.CAN_FilterActivation=ENABLE;

      CAN_FilterInit(&CAN_FilterInitStructure);

    }

    lg michi

    smart2
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:45

    Nobody can help you unless you give some more detail about your code,