CAN1 TX sending continuous messages
Hello,
I have 2 CAN nodes ( both are nucleo f446re boards) and both connected to separate transceivers .
I am exploring CAN_Networking ( NORMAL MODE) given in the ST example .
even if i Tx only one time, the Transmitter sending continuous same messages, and receiver node continuously getting Rx interrupt .
i have connected CANH ( NODE 1 ) ---> CANH(NODE2) , CANL(NODE 1) ---> CANL(NODE 2 ) using jumper wires.
also in the documentation it is mentioned that bus has to be terminated with 120ohm resistor which i have not used. is that causing any issues. ? can anyone please help me understand the problem ?
Thank you
#stm32-discovery