Skip to main content
trevor1
Associate III
May 17, 2009
Question

CAN with internal oscillator

  • May 17, 2009
  • 4 replies
  • 1753 views
Posted on May 17, 2009 at 16:37

CAN with internal oscillator

    This topic has been closed for replies.

    4 replies

    trevor1
    trevor1Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    Hi,

    Is an external crystal required to use CAN (as is the case with USB) or can I use the internal oscillator? The documentation I've read does not mention that a crystal is required.

    Thanks

    Trevor

    trevor1
    trevor1Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    Thanks Todd. I'll go with a crystal then.

    tberk1
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    I had wondered this as well, and found in the BOSCH CAN Bus spec found in a link from wikipedia the following:

    ''A maximum oscillator tolerance of 1.58% is given and therefore the use of a ceramic

    resonator at a bus speed of up to 125 Kbits/s as a rule of thumb''

    ''For the full bus speed range of the CAN protocol, a quartz oscillator is required. ''

    Therefore I would run w/ a quartz crystal.

    Todd

    amin2
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:00

    The STM32 bxCAN is connected to PCLK1 (APB1 clock ) : 36 MHz max