A
Anonymous
March 27, 2023
Solved
CAN transceiver on stm32f407 discovery
- 4 replies
- 3320 views
Hello dear friends,
It's been a week since I worked on the CAN transceiver and couldn't make it work. I have set up the chip rcc, bit rate, and receive interrupt of CAN, set the receive filter, and the receiver id in transmission, with no success. I have used only a single board and connected Tx to Rx (PB8 PB9) through a jumper. I have checked that there is some signal on the Tx line with a voltmeter(Sadly I have no oscilloscope now to check the absolute signals.)
What I am looking for is that I can get the receive interrupt.
I am not going to use the software loop-back mood since I'm not going to use simulation.
The code is attached. Help me what had make it not