Skip to main content
Russ1
Associate
December 9, 2021
Question

Can the STM32F,H Mix 2 I2S channels?

I have a project that requires 2 I2S inputs (4 audio channels) to be level controlled, then mixed into the left channel of an I2S output. 32 bit word length 24 bit samples. I was contemplating using an STM32F or STM32H on a nucleo board to start. Can some kind engineer confirm that this is possible?

Thanks

-russ

This topic has been closed for replies.

1 reply

waclawek.jan
Super User
December 10, 2021

If the sampling rates are identical, yes.

You can estimate it yourself - say you run at 48ksps, with each sample you need to load, multiply, add, that's 3 cycles each i.e. 12 cycles total, then result has to be stored, one additional cycle. Let's add another dozen of cycles for loop management, address calculation etc., that's 25, so around 1.2M instruction cycles per second, if you do things right. That's ample for any 32-bitter, leaving margin for error, other processes, and then some more.

Get a model with enough SAI - the SPI/I2S are quite some pain due to being 16-bit and I2S endianness is big.

There are DISCO board with on-board CODEC, e.g. 'F411 and 'F412.

JW