Skip to main content
DrDro
Associate III
Feb 23, 2024 1:39 PM UTC
Question

Can the rising signal 'hrtim_upd_en1' come directly from software?

Hallo,

I have to use shadow registers (PREEN=1) in HRTIM slave timers.

I have decided to use following configuration:

UPDGAT = 0110: the update occurs on the update event following a rising edge of HRTIM update enable input 1 (hrtim_upd_en1) to perfectly synchronise registry update after software command.

 

I want to evoke "hrtim_upd_en1" directly from software.

I hope that TIM16.EGR registry should allow it exclusively, even without running TIM16 counter.

Am I wrong?

This topic has been closed for replies.

3 replies

Pierre_Paris
ST Employee
Feb 29, 2024 10:43 AM UTC

Hello @DrDro,

Thanks for your question!

First, a short reminder : "when the preload mode is enabled, accessed registers are shadow registers. Their content
is transferred into the active register after an update request, either software or synchronized with an event." (page 1545 of RM0399)

You configured UPDGAT = 0110, the update is done on the update event following a request on the update enable input 1..3 (the event can be enabled with TxREPU, MSTU or TxU).

If you want to update from software, I suggest you to directly write 1 into TxSWU bit in HRTIM_CR2.

Best Regards,

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DrDro
DrDroAuthor
Associate III
Mar 4, 2024 6:33 AM UTC

Thank you, Pierre,

 

yes, that is the easiest way using TxSWU.

You have expresed here very clearly "update event" and "update request". This helps a lot to understand the logic behind. In RM it is not so obvious. Thanks a lot for this disambiguation.

However, transfering shadow registers immediate on TxSWU is not good solution for me, I need a seguence: update on the update event (timer reset) following the request (software write).

Greetings

Pierre_Paris
ST Employee
Mar 4, 2024 9:46 AM UTC

Hello @DrDro,

When the preload is enabled (PREEN bit set), there are 3 use cases :

  1. The update is done independently from DMA burst transfers
  2. The update is done when the DMA burst transfer is completed
  3. The update is done on the update event following the DMA burst transfer completion

If you want to update registers on the timer reset, you should have a look on this figure (especially the option 2) :

Pierre_Paris_0-1709544411414.png

Did I answer your question ? 

Best Regards,

Pierre

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.