Skip to main content
MPicc
Associate
Jun 27, 2019 6:15 PM UTC
Question

Can the ADCs on the STM32F767 be configured in differential input mode?

In some of the tutorial materials it mentions that the ADCs on the STM32F7 devices can be used in single-ended or differential input modes. I have studied the reference manual but have had no luck in defining how to use the STM32F767's ADC in differential input mode. Am I missing something, and if so can someone point me in the right direction towards accomplishing differential input mode on this device.

Thanks in advance!

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
Jun 27, 2019 7:36 PM UTC

> In some of the tutorial materials

Namely?

AFAIK, differential mode is on only in ADC of 'F3, 'L4 and 'H7 (probably also the new 'G4, I did not check that).

JW

MPicc
MPiccAuthor
Associate
Jun 27, 2019 7:43 PM UTC

Mentioned in link below on "STM32F7 Online Training" slide 3. Thanks for the clarification.

https://st-onlinetraining.s3.amazonaws.com/STM32F7-Analog_ADC/index.html