Question
can't set reset a Bit (STM32F091 64pins)
Posted on May 04, 2015 at 11:49
Hello everyone.
My target is STM32F091C I want to send something using SPI and after that make an impulse with a bit of my microcontroller. On my scope I see that I send well the data but the impulse is not generate. Here is the code of the gpio init + the function that should generate the impulse : void init_system_gpio (void) { GPIO_InitTypeDef GPIOA_Init; GPIO_InitTypeDef GPIOB_Init; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOB,ENABLE); /*PORT B and PORT A are used*/ /*PORT B Configuration*/ GPIOB_Init.GPIO_Pin =GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7 | GPIO_Pin_13 | GPIO_Pin_15; GPIOB_Init.GPIO_Speed = GPIO_Speed_50MHz; GPIOB_Init.GPIO_Mode = GPIO_Mode_AF; GPIOB_Init.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIOB_Init.GPIO_OType = GPIO_OType_PP; GPIO_Init(GPIOB, &GPIOB_Init); GPIO_PinAFConfig(GPIOB, GPIO_PinSource3, GPIO_Mode_OUT); //Freq_UPD GPIO_PinAFConfig(GPIOB, GPIO_PinSource4, GPIO_Mode_OUT); //LED Debug 1 GPIO_PinAFConfig(GPIOB, GPIO_PinSource5, GPIO_Mode_OUT); //LED Debug 2 GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_Mode_IN); //BP1 GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_Mode_IN); //BP2 GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_0); //SPI2 CLK GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_0); //SPI2 MOSI /*PORT A Configuration*/ GPIOA_Init.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_4 | GPIO_Pin_9| GPIO_Pin_10 | GPIO_Pin_15; GPIOA_Init.GPIO_Speed = GPIO_Speed_50MHz; GPIOA_Init.GPIO_Mode = GPIO_Mode_AF; GPIOA_Init.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIOA_Init.GPIO_OType = GPIO_OType_PP; GPIO_Init(GPIOA, &GPIOA_Init); GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_Mode_AN); //ADC_IN0 GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_Mode_AN); //DAC_OUT1 GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_0); //UART1 TX GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_0); //UART1_RX GPIO_PinAFConfig(GPIOA, GPIO_PinSource15, GPIO_Mode_OUT);//RST DDS } void freq_ud_dds(void){ GPIOB->ODR=(GPIOB->ODR)|0x04; // int i =0; // GPIO_WriteBit(GPIOB, GPIO_Pin_3, Bit_SET); // while(i<200) i++; // GPIO_WriteBit(GPIOB, GPIO_Pin_3, Bit_RESET); // GPIO_SetBits(GPIOB, GPIO_Pin_3); // GPIO_ResetBits(GPIOB, GPIO_Pin_3); }; As you can see in this last function I tried many ways to set/reset my bit... If you can help me to generate this pulse, it would be great ! Thank you