Skip to main content
davebell9
Associate II
October 19, 2010
Question

Can't seem to build & launch anything (Atollic TrueSTUDIO lite)

  • October 19, 2010
  • 11 replies
  • 2747 views
Posted on October 19, 2010 at 21:40

Total noob at this, trying to (re-)build and launch the demo code on the Discovery board as a baseline.

I'm running under Windows XP, downloaded and installed 

Atollic TrueSTUDIO lite.

Discovery board is connected via USB cable, and happily runs its default program.

I succeeded in opening and (at least apparently) building the project, but what now?

When I select Run, I get ''Unable To Launch: The selection cannot be launched, and there are no recent launches.'' popup.

Is there a simple, clear, step-by-step beginner's guide to operating the tools?

Thanks!

Dave

    This topic has been closed for replies.

    11 replies

    Tesla DeLorean
    Guru
    October 22, 2010
    Posted on October 22, 2010 at 20:37

    Does that sound right?

    Yes, the straight download is buggy, I think it is the driver or the API. If you want to flash some arbitrary data the ST-LINK Utility program works better.

    This is the only ST-LINK target I have, most everything else I'm using a U-Link (1/2/ME)

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..