Skip to main content
Associate
August 8, 2025
Question

Can't erase external flash sector on a B-U585I-IOT02A board with STM32CubeIDE functions.

I'm trying unsuccessfully to erase a 4K sector at 0x73ff0000 using STM32CubeIDE code, but the STM32CubeProgrammer works fine.  I've tried using BSP_OSPI_NOR_Erase_Block() and MX25LM51245G_BlockErase() with no luck.

My code base is the HTTP_IOT_WebServer example.  My basic code is (where addr=0x73FF0000 and EFLASH_SECTOR_MASK=0x03FFF000)

 -------------------------------------------

BSP_OSPI_NOR_DisableMemoryMappedMode(0);

 

rc = MX25LM51245G_BlockErase(&hospi_nor[0], MX25LM51245G_SPI_MODE, MX25LM51245G_STR_TRANSFER,

HAL_OSPI_ADDRESS_32_BITS, addr & EFLASH_SECTOR_MASK,

MX25LM51245G_ERASE_4K);

 

BSP_OSPI_NOR_DisableMemoryMappedMode(0);

 -------------------------------------------

Any idea why this doesn't work? Is the Programmer doing anything I'm not doing?

 

-Marty

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
August 8, 2025

Read the Status Register, and check the BPB (Block Protection Bits)

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MartyAuthor
Associate
August 11, 2025

Status Reg = 0x00 before and after attempt to erase.  The BP0-BP3 bits are zero, no protection.

-Marty

Tesla DeLorean
Guru
August 11, 2025

>>Any idea why this doesn't work? Is the Programmer doing anything I'm not doing?

The memory is not in the mode you think it is?

ie Not in SPI mode, not in 32-bit mode

Look at what exactly is being sent. Describe the nature of the failure. Does it complete immediately? Ignore the command? Not erase? Not respond to other commands?

You've sent a Write Enable? It spends some time in Wait for Complete? A 64KB sector erase at a 64 KB boundary? Zero-Basis address?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MartyAuthor
Associate
September 27, 2025

Sorry for the late (ok lack of) reply, but I never truly resolved this.  It appeared that after a "successful" erase the memory did not show up as all 0xFF's as I expected, so seemingly un-erased. However reprogramming apparently worked.  So on an Erase I erased then reprogrammed to 0xFF's for visibility, and on Program I erased then programmed what I wanted.  That worked OK.