Can STM32F103RB-Nucleo even do PWM Input Capture?
Cannot get it to fire the IC Capture interrupt, and the macro that decodes the PWM Pulse finished interrupt might be broken becuase all running timers seem to be sent a handle to that callback. htim->Instance TIM2 gets a callback, when i tried.
LED shows the PWM ringing away from TIM1 but TIM2 never gets the IC Capture callback
STM32CubeMX 4.22
STM32Cube_F1_1.6
Timer 1:
prescaler 7199
period 9999
pulse 5
Output to pin PA11
Timer 2:
prescaler 0
period 65535
input TI1FP1 on PA0
The CubeMX application generates:
/**TIM2 GPIO Configuration
PA0-WKUP ------> TIM2_CH1 */ GPIO_InitStruct.Pin = GPIO_PIN_0; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL;and GPIO_MODE_AF_INPUT is the same as MODE_INPUT
DIER is set for interrupt on CC1IE and CC2IE
can't get CCR1 to set
Registers:
AFIO->MAPR: 0x02000000
GPIOA->CRL: 0x4434AA44
GPIOA->CRH: 0x8884B444GPIOA->IDR: 0x0000F7DEGPIOA->ODR: 0x0000A000GPIOA->BSRR: 0x00000000GPIOA->BRR: 0x00000000GPIOA->LCKR: 0x00000000TIM1->CR1: 0x00000001
TIM1->CR2: 0x00000000TIM1->PSC: 0x00001C1FTIM1->ARR: 0x0000270FTIM1->RCR: 0x00000000TIM1->DIER: 0x00000010TIM1->SMCR: 0x00000000TIM1->CCER: 0x00001000TIM1->CCMR1: 0x00000000TIM1->CCMR2: 0x00006C00TIM1->CCR1: 0x00000000TIM1->CCR2: 0x00000000TIM1->CCR3: 0x00000000TIM1->CCR4: 0x00000005TIM1->EGR: 0x00000000TIM1->DCR: 0x00000000TIM1->DMAR: 0x00000001TIM1->CNT: 0x0000027BTIM1->SR: 0x00000011TIM2->CR1: 0x00000001
TIM2->CR2: 0x00000000TIM2->PSC: 0x00000000TIM2->ARR: 0x0000FFFFTIM2->RCR: 0x00000000TIM2->DIER: 0x00000006TIM2->SMCR: 0x00000054TIM2->CCER: 0x00000002TIM2->CCMR1: 0x00000201TIM2->CCMR2: 0x00000000TIM2->CCR1: 0x00000000TIM2->CCR2: 0x00000000TIM2->CCR3: 0x00000000TIM2->CCR4: 0x00000000TIM2->EGR: 0x00000000TIM2->DCR: 0x00000000TIM2->DMAR: 0x00000001TIM2->CNT: 0x00005821TIM2->SR: 0x00000059