Skip to main content
JSerr.441
Associate
August 17, 2020
Question

CAN Rx Interrupt cannot be reactivated due to LOCKED using HAL_CAN during Tx in Background

  • August 17, 2020
  • 0 replies
  • 426 views

 We use HAL_CAN_Transmit in the application. If during the call of this function a CAN Rx Interrupt happens, in the function void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef* opt_canHandler) the HAL_CAN_Receive_IT fails as the CAN is is still HAL_LOCKED. We have disabled the CAN Interrupt during the Tx process, but as we Need a large timeout on the TX because a high bus load, then we get a FOV Fifo overrun failre on RX. Is it possible to just unlock the CAN in the Interrupt or is the only solution to use Tx also in Interrupt? Can a Rx Interrupt Interrupt an Rx Interrupt? Many thanks for the help, Jaume

This topic has been closed for replies.