Skip to main content
Sawd
Visitor II
February 10, 2023
Question

Can one use the same .hex file to program both the STM32F446RET6 and STM32F446RCT6?

  • February 10, 2023
  • 1 reply
  • 596 views

The STM32F446RET6 and STM32F446RCT6 are similar except for Flash size. Is it possible to create a .hex file that programs the RE version that could program both chips using the ST-Link V2?

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
February 10, 2023

If the image fits in the smaller flash you should be able to create a single image.

The flash size is in a variable you can recover from the System/OTP memory space.

The size frequently refers to how much of the flash memory on the die was tested, as this is a significant cost in terms of test time and throughput.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..