Skip to main content
Pzhu.1
Associate II
Oct 22, 2020 1:59 AM UTC
Solved

Can not write data in flash of STM32G030C8T6

This is my code;it when run to the code in the picture, the MCU will deadvoid Flash_Test(void)

{

  U32  Write_Addr = FLASH_USER_START_ADDR; //FLASH_USER_START_ADDR=((uint32_t)0x0800E000)

  uint64_t data64=0x1234567812345678;

  EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;

  EraseInitStruct.Page = FLASH_USER_START_ADDR;

  EraseInitStruct.NbPages = (FLASH_USER_END_ADDR - FLASH_USER_START_ADDR) / FLASH_PAGE_SIZE;

  HAL_FLASH_Unlock();

   if (HAL_FLASHEx_Erase(&EraseInitStruct, &PageError) != HAL_OK)

   {

     //HAL_FLASH_Lock();

     // return 0;----

   }

   HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, Write_Addr, data64);

} 

This topic has been closed for replies.
TDK
TDKBest answer
Oct 22, 2020 2:27 AM UTC

>  EraseInitStruct.Page = FLASH_USER_START_ADDR;

Pretty sure page should be an integer between 0 and the number of pages, not an address.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
Oct 22, 2020 2:27 AM UTC

>  EraseInitStruct.Page = FLASH_USER_START_ADDR;

Pretty sure page should be an integer between 0 and the number of pages, not an address.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pzhu.1
Pzhu.1Author
Associate II
Oct 22, 2020 3:31 AM UTC

Thanks very much!!!​