Skip to main content
Associate
January 28, 2024
Question

Can not read memory! Disable Read out protection and retry

  • January 28, 2024
  • 1 reply
  • 2024 views

Hello. I have an STM32F407 development board. While I was getting used to this card last week, the card put itself into memory read protection. When I try to debug or throw code, the attached warning appears and the attached Fail file is created. Even though I try to set the RDP level to Level 0 (AA) in the "option bytes" option with the STLink utility and STMCube Programmer, it does not work. and the same warning happens again. RDP level appears as FF in STMCube Programmer. I looked at all the form sites. I did all the suggestions but it didn't work (updating STMutility, etc.). How can this situation be corrected? Has anyone experienced this situation before? Can you help?

ramazan_kavak_0-1706471661684.jpeg

 

ramazan_kavak_1-1706471661687.jpeg

 

ramazan_kavak_2-1706471661688.jpeg

 

ramazan_kavak_3-1706471661690.jpeg

 

ramazan_kavak_4-1706471661694.jpeg

 

ramazan_kavak_5-1706471661696.jpeg

 

 

This topic has been closed for replies.

1 reply

STOne-32
ST Technical Moderator
January 28, 2024

Dear @ramazan_kavak ,

 

Welcome in our STCommunity ! 

based on the described symptoms it seems a hardware problem caused by non correct loading of the Options Bytes ( factory programmed) and non user.  Here is what I suggest you for a sanity check :

1) Apply a Reset and if you have the possibility to measure the current consumption of IDD and compare it versus normal operation .

2) Apply a PDR and POR , Power down and then power On

3) please check the V12 on VCAP pins and also the value of the capacitors we should have 2,2uF

4) a hint , if possible to try to heat the device ( while VDD is off , including all board) as you desolder it and then solder it again with a rework station and not exceed the specs - if using PbFree around <300 degree .  I know it is complex but give a try as best as you can .


5) if possible to have the top marking of the device - a top picture is fine . 

Hope it helps you .

Cheers,

STOne-32