CAN message not sent.
Hi! CAN message not sent. Please see where I'm wrong?
int main (void){
SysClock();
CanInit();
CanFilter();
CAN_ConfigInterupt();
while(1)
{
TransmitMsg();
delay(100);
}
}
void CanInit (void){
//PA12 - CAN=TX
//PA11 - CAN-RX
RCC->APB2ENR |= RCC_APB2ENR_IOPAEN;
RCC->APB2ENR |= RCC_APB2ENR_AFIOEN;
RCC->APB1ENR |= RCC_APB1ENR_CAN1EN;
GPIOA->CRH |= GPIO_CRH_CNF11_1; //Input with pull-up / pull-down
GPIOA->CRH &= ~GPIO_CRH_MODE11; //Input mode (reset state)
GPIOA->CRH |= GPIO_CRH_CNF12_1; //Alternate function output Push-pull
GPIOA->CRH |= GPIO_CRH_MODE12; //Output mode, max speed 50 MHz.
AFIO->MAPR &= ~AFIO_MAPR_CAN_REMAP;
CAN1->MCR |= CAN_MCR_INRQ;
while(!(CAN1->MSR & CAN_MSR_INAK));
CAN1->MCR &= ~CAN_MCR_TTCM;
CAN1->MCR &= ~CAN_MCR_ABOM;
CAN1->MCR &= ~CAN_MCR_AWUM;
CAN1->MCR &= ~CAN_MCR_NART;
CAN1->MCR &= ~CAN_MCR_RFLM;
CAN1->MCR &= ~CAN_MCR_TXFP;
/******************** 500kbit/s ***************************/
CAN1->BTR = 0;
CAN1->BTR |= (3 << 0) BRP 3
| (11 << 16) //TS1 = 11
| (4 << 20) //TS2 = 4
| (2 << 24) //SJW = 2
| (1 << 30) //Loop Back Mode enabled
| (1 << 31); //Silent Mode
/************************************************************************/
CAN1->MCR &= ~CAN_MCR_INRQ;
while(CAN1->MSR & CAN_MSR_INAK);
}
void CanFilter(void)
{
CAN1->FMR |= CAN_FMR_FINIT;
CAN1->FMR |= CAN_FMR_CAN2SB;
CAN1->FM1R &= ~CAN_FM1R_FBM0;
CAN1->FS1R = CAN_FS1R_FSC0;
CAN1->FFA1R = 0x00;
CAN1->sFilterRegister[0].FR1 = 0x0;
CAN1->sFilterRegister[0].FR2 = 0x0;
CAN1->FA1R = CAN_FA1R_FACT0;
CAN1->FMR &= ~CAN_FMR_FINIT;
}
void TransmitMsg(void)
{
uint8_t Data[8];
Data[0] = 1;
Data[1] = 2;
Data[2] = 3;
Data[3] = 4;
Data[4] = 5;
Data[5] = 6;
Data[6] = 7;
Data[7] = 8;
CAN1->sTxMailBox[0].TIR |= (0x222 << 21);
CAN1->sTxMailBox[0].TDTR &= 0xFFFFFFF0U;
CAN1->sTxMailBox[0].TDTR |= 8;
CAN1->sTxMailBox[0].TDLR |= (((uint32_t)Data[3] << (24U)) |
((uint32_t)Data[2] << (16U)) |
((uint32_t)Data[1] << (8U)) |
((uint32_t)Data[0] << (0U)));
CAN1->sTxMailBox[0].TDHR |= (((uint32_t)Data[7] << CAN_TDL0R_DATA3_Pos) |
((uint32_t)Data[6] << CAN_TDL0R_DATA2_Pos) |
((uint32_t)Data[5] << CAN_TDL0R_DATA1_Pos) |
((uint32_t)Data[4] << CAN_TDL0R_DATA0_Pos));
CAN1->sTxMailBox[0].TIR |= CAN_TI0R_TXRQ;
}