Skip to main content
LMiya
Associate
November 7, 2018
Question

Can I use two SPIs as a master and slave in one board? (Nucleo-L432KC)

  • November 7, 2018
  • 2 replies
  • 1064 views

I'm testing my small project using SPI.

In that project, the board, Nucleo-L432KC (used as a mbed board), has to receive data from a SPI master as a SPI slave, and send processed data to another device as a SPI master.

Then, the board has to work as a SPI slave and a SPI master at the same time.

Nucleo-L432KC has 2 SPI (SPI1 and SPI3) and so I tried to configure both of them, but SCLK output as a master didn't work.

Is it possible to use 2 SPI as a master and a slave?

Configuration

 SPI1 as a slave

 using MOSI = A6, MISO = A5, SCLK = A4, SSEL = D3

 format:(8,3), frequency:6750000

 SPI3 as a master

 using MOSI = D11, MISO = D12, SCLK = D13, SSEL = D9

 format:(8,3), frequency:6750000

 If they are not configured at the same time, it seems to work well.

a part of my code:

 SPI_3_SSEL = 1;
 spi_3.format(SPI_3_BITS, SPI_3_MODE);
 spi_3.frequency(SPI_3_FREQ);
 SPI3->CR1 &= ~0x80; //MSBFirst
 
 
 
 spi_1.format(SPI_1_BITS, SPI_1_MODE);
 spi_1.frequency(SPI_1_FREQ);
 SPI1->CR1 |= 0x80; //LSBFirst
 SPI1->CR2 |= 0x40; //Interrupt
 NVIC_SetVector(SPI1_IRQn, (uint32_t) &intrrptSPI1); //Callback function
 NVIC_SetPriority(SPI1_IRQn, 1); //Priority
 NVIC_EnableIRQ(SPI1_IRQn); //Enable interrupt

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
November 7, 2018

> If they are not configured at the same time, it seems to work well.

Read out the content of SPI and relevant GPIO registers - both when configured separately and working, and when configured together and not working - and compare them.

JW

LMiya
LMiyaAuthor
Associate
November 7, 2018

Thank you for your advice!

I checked SPI registers and they were following.

only SPI1

SPI1 CR1:00db

SPI1 CR2:1740

SPI1 SR:00c2 or 0082 or 0042 or 0002

SPI3 CR1:0000

SPI3 CR2:0000

SPI3 SR:0000

only SPI3

SPI1 CR1:035f

SPI1 CR2:1700

SPI1 SR:00c2 or 0082 or 0042 or 0002

SPI3 CR1:0000

SPI3 CR2:0000

SPI3 SR:0000

both SPI1 and SPI3

SPI1 CR1:00db

SPI1 CR2:1740

SPI1 SR:00c2 or 0082 or 0042 or 0002

SPI3 CR1:0000

SPI3 CR2:0000

SPI3 SR:0000

​(The value of SPI1-SR changed at each trial.)

It implys that SPI3 is not used??

I thought the number of SPI is determined by PIN number for MOSI, MISO, SCLK, but that's wrong?

In my code, I define SPIs as following.

const int SPI_3_BITS = 8;
const int SPI_3_MODE = 3;
const int SPI_3_FREQ = 6750000;
const PinName SPI_3_MOSI = D11;
const PinName SPI_3_MISO = D12;
const PinName SPI_3_SCK = D13;
DigitalOut SPI_3_SSEL(D9);
SPI spi_3(SPI_3_MOSI, SPI_3_MISO, SPI_3_SCK);
 
const int SPI_1_BITS = 8;
const int SPI_1_MODE = 3;
const int SPI_1_FREQ = 6750000;
const PinName SPI_1_MOSI = A6;
const PinName SPI_1_MISO = A5;
const PinName SPI_1_SCK = A4;
const PinName SPI_1_SSEL = D3;
SPISlave spi_1(SPI_1_MOSI, SPI_1_MISO, SPI_1_SCK, SPI_1_SSEL);

Thank you in advance