Hi, @Siniša Marović
no, according to the RM0433, section 2.4 Embedded SRAM the largest contigouos SRAM block is the AXI one at 0x2400'0000 with a size of 0x8'0000 (512K). You will also find some gaps called Reserved between some of the blocks, which makes it impossible to address the entire 1MB as one block - it also contains ITCM/DTCM and Backup RAM.
Maybe you should consider to use the STM32H7B0 or STM32H7A3 which provide 1MB AXI SRAM?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.