Question
Can I slave STM32s off of a master STM32 crystal clock oscillator ?
I want to have one STM32F730 using a crystal on OSCIN and OSCOUT, and then slave 7 other STM32F730s to the same clock. But if I connect OSCIN of these other 7 to OSCOUT of processor 1 I assume it will load that pin with too much capacitance. I can't see a way of getting a buffered clock out at the crystal frequency fHSE to drive the other processors so do I have to add an external buffer ?