Skip to main content
Ehill.16
Senior
December 5, 2019
Question

Can I remove the on board display and use the Newhaven display with this development board?

  • December 5, 2019
  • 3 replies
  • 760 views

Can I remove the on board display and use the Newhaven display with this development board?

    This topic has been closed for replies.

    3 replies

    S.Ma
    Principal
    December 5, 2019

    How about this one?

    Tesla DeLorean
    Guru
    December 5, 2019

    "Can I remove the on board display and use the Newhaven display with this development board?"

    What development board? Provide context, your post is far too vague and non-specific.

    https://community.st.com/s/question/0D50X0000BfuZ3iSQE/stm32f746gdisco-question

    You will need to do the due-diligence on this. Review the circuits and signalling expectations.

    If you can't make these determinations from available documentation, the answer is probably No, and you'll likely need to do the experiment and work up the code to come to a definitive answer. Or pay going rates for someone else to do the work.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Ehill.16
    Ehill.16Author
    Senior
    December 5, 2019

    I'm using the STM32F429 Discovery board. I see from the schematic of this board that it is using a 18 bit RGB interface which is fine. Also, it looks like the LCD is connected via a 48 pin FFC connector.