Skip to main content
ikassma
Associate III
Mar 19, 2019 6:45 AM UTC
Question

Can i get St-link Utility External Flash loader source code?

hi dear.

I built a custom board based on the Stm32f796i-discovery Board.

I am trying to link TouchGFX but I can not write image to External Flash Memory (MX25L5124G).

The MX25L512G_STM32F769I-DISCO.stldr file is located in the External Loader folder of the ST-link utility.

I am sure someone will have an IAR Project for this file.

Can I get the IAR Project file for this file?

This topic has been closed for replies.

7 replies

Imen Ezzine
ST Employee
Aug 7, 2020 2:25 PM UTC

Hi ikassma,

I will woulk your request internally and see If I can come back with the the IAR Project you need for MX25L512G_STM32F769I-DISCO.stldr.

-Imen

ikassma
ikassmaAuthor
Associate III
Aug 8, 2020 12:12 AM UTC

thank you for your answer. if you can send iar project file at to my e mail address

Imen Ezzine
ST Employee
Aug 10, 2020 11:22 AM UTC

Hi ikassma,

I did check for you and unfortunately I couldn't find the code source on IAR.

What I can suggest to you is to take a look at STM32F769 Firmware (here) under Drivers/BSP. You will find the QSPI drivers needed for the STM32F769I-Discovery board. You can include these files (.c/.h) in your project or just use the needed functions to perform actions to the External Flash Memory (write etc...)

I hope this help!

-Imen