Skip to main content
mamellas
Associate
May 10, 2019 10:28 AM UTC
Solved

Can i do an hexapod with facial recognizer with just a STM?

Hi, for my thesis i'd like to do an hexapod(it'll have like 14 servos) and a camera for facial recognizer. I was thinking about an arduino for the control of the robot and a pi3 for the facial recognizer, and then stm32 came to me. Will I be able to do the previously presented with just a STM microcontroller or microprocessor, if it's possible which one would be?

Thanks in advance.

    This topic has been closed for replies.
    MikeDB
    MikeDBBest answer
    Senior II
    May 10, 2019 12:28 PM UTC

    Any STM will replace the Arduino happily - look up Blue Pill modules which are about a $1. It even runs Arduino code if you want.

    For the pi3, you'll need the new MP1 which are still in short supply, and more expensive than the pi. I'd stick with the pi for that part. With a highly optimised algorithm you possibly could scrape by with a H7 but once you add all the memory and so on, the pi3 becomes cheaper again.

    3 replies

    MikeDB
    MikeDBBest answer
    Senior II
    May 10, 2019 12:28 PM UTC

    Any STM will replace the Arduino happily - look up Blue Pill modules which are about a $1. It even runs Arduino code if you want.

    For the pi3, you'll need the new MP1 which are still in short supply, and more expensive than the pi. I'd stick with the pi for that part. With a highly optimised algorithm you possibly could scrape by with a H7 but once you add all the memory and so on, the pi3 becomes cheaper again.

    mamellas
    mamellasAuthor
    Associate
    May 10, 2019 12:38 PM UTC

    I'll check the Blue Pill, and stick with the pi. Thank you so much!

    MikeDB
    Senior II
    May 10, 2019 12:40 PM UTC