Skip to main content
Associate III
May 28, 2024
Solved

CAN Communication in Loopback mode with STM32F407

I want to implement CAN Communication in Loopback mode in which I have added Can interrupt mode . In Tx interrupt it will sent data after every 1000 m/s and data increment . In Rx interrupt it will read the sent data. I compiled the code and it will show me the value in live registers.  But I am not able to see that in logic analyzer. Suggest me some ideas to help me out.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
May 28, 2024

Hello,

What config you have enabled?

This one:

SofLit_0-1716928168605.png

or this one:

SofLit_1-1716928196501.png

Or this one?

SofLit_2-1716928249621.png

You need to select the second one and configure the correct GPIO pin.

And don't forget to enable the pull-up for Rx pin.

Otherwise you need to share your project for an efficient help.

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

3 replies

Karl Yamashita
Principal
May 28, 2024

You haven't said which CAN controller and the port pin you're monitoring. Is the CAN transceiver in place and are you connected to other CAN nodes? If so, are you probing before or after the CAN transceiver? If it's after the Transceiver, is the RS pin pulled low?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
May 28, 2024

Hello,

What config you have enabled?

This one:

SofLit_0-1716928168605.png

or this one:

SofLit_1-1716928196501.png

Or this one?

SofLit_2-1716928249621.png

You need to select the second one and configure the correct GPIO pin.

And don't forget to enable the pull-up for Rx pin.

Otherwise you need to share your project for an efficient help.

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Visitor II
October 28, 2024

can pls post your source code here.