Skip to main content
swordkillers
Visitor II
November 27, 2013
Question

CAN cannot enter RX interrupt when ADC enabled

  • November 27, 2013
  • 0 replies
  • 418 views
Posted on November 27, 2013 at 15:13

Hi eveveryone,

I met a very strange problem in STM32F103VC. I used PB8 and PB9 for CAN, PA6 and PA7 for 2 channel ADC. The CAN communication use interrrupt mode, ADC use query mode. If I only use CAN, it works well, any message in CAN bus will generate RX interrupt; and if only ADC, it works well, I can get the voltage. But if I make them work togother, the ADC works well, the CAN cannot goto RX interrupt, but if I send message to the CAN bus, the CAN can goto RX interrupt once.

This is my code.

//////////////////////////////////////////////

void NVIC_Configuration(void)

{

NVIC_InitTypeDef NVIC_InitStructure; //???????

&sharpifdef  VECT_TAB_RAM

/* Set the Vector Table base location at 0x20000000 */

NVIC_SetVectorTable(NVIC_VectTab_RAM, 0x0);

&sharpelse  /* VECT_TAB_FLASH  */

/* Set the Vector Table base location at 0x08000000 */

NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x0);

&sharpendif

NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);//

//enable USART interrupt

NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;  

NVIC_Init(&NVIC_InitStructure); //

/* Enable CAN1 RX0 interrupt IRQ channel */

NVIC_InitStructure.NVIC_IRQChannel = USB_LP_CAN1_RX0_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 2;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

//enable TIM2 interrupt

NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 3;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

/*

//enable TIM3 interrupt

NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 4;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

*/

}

/********* CAN Configuration*************************/

void CAN_GPIO_Configuration(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

/* CAN Periph clock enable */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO ,ENABLE);

RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);

GPIO_PinRemapConfig(GPIO_Remap1_CAN1,ENABLE); 

/* Configure CAN pin: RX */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;//GPIO_Mode_IN_FLOATING;

GPIO_Init(GPIOB, &GPIO_InitStructure);   

/* Configure CAN pin: TX */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

GPIO_Init(GPIOB, &GPIO_InitStructure);     

}

void CAN_Configuration(void)

{

CAN_InitTypeDef        CAN_InitStructure;

CAN_FilterInitTypeDef  CAN_FilterInitStructure;

CAN_GPIO_Configuration();

/* CAN register init */

CAN_DeInit(CAN1);

CAN_StructInit(&CAN_InitStructure);

/* CAN cell init */

CAN_InitStructure.CAN_TTCM = DISABLE;

CAN_InitStructure.CAN_ABOM = DISABLE;

CAN_InitStructure.CAN_AWUM = DISABLE;

CAN_InitStructure.CAN_NART = DISABLE;

CAN_InitStructure.CAN_RFLM = DISABLE;

CAN_InitStructure.CAN_TXFP = ENABLE;

CAN_InitStructure.CAN_Mode = CAN_Mode_Normal;

CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;

CAN_InitStructure.CAN_BS1 = CAN_BS1_3tq;

CAN_InitStructure.CAN_BS2 = CAN_BS2_2tq;

CAN_InitStructure.CAN_Prescaler = 6; //1MHz

if (CAN_Init(CAN1,&CAN_InitStructure) == CANINITFAILED)

{

}

CAN_FilterInitStructure.CAN_FilterNumber=0;

CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdMask;

CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_32bit;

CAN_FilterInitStructure.CAN_FilterIdHigh=0x0000;

CAN_FilterInitStructure.CAN_FilterIdLow=0x0000;

CAN_FilterInitStructure.CAN_FilterMaskIdHigh=0x0000;

CAN_FilterInitStructure.CAN_FilterMaskIdLow=0x0000;

CAN_FilterInitStructure.CAN_FilterFIFOAssignment=0;

CAN_FilterInitStructure.CAN_FilterActivation=ENABLE;

CAN_ITConfig(CAN1,CAN_IT_FMP0, ENABLE);

CAN_FilterInit(&CAN_FilterInitStructure);

}

/************ ADC configuration ***************************/

void ADC_Configuration(void)

{

ADC_InitTypeDef ADC_InitStructure;   

GPIO_InitTypeDef GPIO_InitStructure;  

RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1 | RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE); // If I disable this line, CAN will enter interrupt

RCC_ADCCLKConfig(RCC_PCLK2_Div6);   

                          

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6|GPIO_Pin_7;  

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;       

GPIO_Init(GPIOA, &GPIO_InitStructure);    

ADC_DeInit(ADC1);  

ADC_InitStructure.ADC_Mode = ADC_Mode_Independent; 

ADC_InitStructure.ADC_ScanConvMode = DISABLE; 

ADC_InitStructure.ADC_ContinuousConvMode = DISABLE; 

ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None; 

ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; 

ADC_InitStructure.ADC_NbrOfChannel = 1; 

ADC_Init(ADC1, &ADC_InitStructure); 

ADC_Cmd(ADC1, ENABLE); 

 

ADC_ResetCalibration(ADC1);

  

while(ADC_GetResetCalibrationStatus(ADC1)); 

 

ADC_StartCalibration(ADC1);  

while(ADC_GetCalibrationStatus(ADC1));

}

u16 ADC_GetVal(ADC_TypeDef *  ADCx, uint8_t  ADC_Channel)

{

u16 adc_val = 0;

ADC_RegularChannelConfig(ADCx, ADC_Channel, 1, ADC_SampleTime_239Cycles5 );                     

ADC_SoftwareStartConvCmd(ADCx, ENABLE);     

  

while(!ADC_GetFlagStatus(ADCx, ADC_FLAG_EOC ));

adc_val = ADC_GetConversionValue(ADCx); 

return adc_val;

}

#stm32-adc-can-interrupt
This topic has been closed for replies.