Skip to main content
HSagh.1
Associate II
May 19, 2024
Solved

CAN bus stop working when cpu is put in sleep (STM32F205VGTX)

On STM32F205VGTX, when I put cpu in sleep by using this command:

 

HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON, PWR_SLEEPENTRY_WFI);

 

CAN peripheral stops working. It does not acknowlege bus messages anymore and there is no CAN interrupts to wake up the cpu.

I had a look at the datasheet, I was not able to find whether CAN is supposed to or not supposed to work in cpu sleep mode.

My question is if this is how it is supposed to be, or I need to do some more to keep CAN alive in this mode.

 

Thanks

This topic has been closed for replies.
HSagh.1
HSagh.1Best answer
Associate II
May 21, 2024

Actually I found the problem. Somewhere hidden in the inititalisation code AxBnLPENR registers were wrongly cleared by a test code that should have been removed. That was the main reason.

I also do not need to enable Autowakeup, becasue I do not put CAN module into SLEEP. I just put cpu into sleep.

2 replies

mƎALLEm
ST Technical Moderator
May 20, 2024

Hell,

Related thread: https://community.st.com/t5/stm32-mcus-products/wake-up-mcu-by-canbus-interruptions-from-sleep-mode-stm32f1/td-p/62564

Did you enable CAN Rx FIFO interrupt?

Did you enable Autowakeup?

Also read "27.4.3 Sleep mode (low-power)" section in RM0033.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
HSagh.1
HSagh.1AuthorBest answer
Associate II
May 21, 2024

Actually I found the problem. Somewhere hidden in the inititalisation code AxBnLPENR registers were wrongly cleared by a test code that should have been removed. That was the main reason.

I also do not need to enable Autowakeup, becasue I do not put CAN module into SLEEP. I just put cpu into sleep.