Skip to main content
leesh
Associate
May 17, 2009
Question

CAN Bit timing Calculation

  • May 17, 2009
  • 3 replies
  • 1322 views
Posted on May 17, 2009 at 15:50

CAN Bit timing Calculation

    This topic has been closed for replies.

    3 replies

    adamajames
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:08

    Dear Amin,

    Can you reattach the xls file as I'm after the correct setting on the STM32F103 for 500kbps and 250kbps CAN.

    I get a bit error every now an then. Do you?

    Regards,

    PB

    amin2
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:08

    your calculation is correct , but you have to respect the standard rule : 8=

    I suggest you to use

    BRP = 149

    TS1 = 7

    TS2 = 2

    attached an xls file tio calculate the Baudrate

    Amin

    [ This message was edited by: amin.agina on 17-05-2009 19:24 ]

    leesh
    leeshAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 13:08

    (RM p510)

    CAN BaudRate = 1 / NominalBitTime

    - NominalBitTim = 1*tq + tBS1 + tBS2

    - tBS1 = tq * (TS1 + 1), tBS2 = tq * (TS2 + 1)

    - tq = (BRP + 1) * tPCLK

    - then...

    - NominalBitTim = 1*tq + tBS1 + tBS2

    = 1*tq + tq * (TS1 + 1) + tq * (TS2 + 1)

    = tq(1 + (TS1 + 1) + (TS2 + 1))

    = tq(3 + TS1 + TS2)

    - if BaudRate = 20K...

    20K = 1 / (tq(3 + TS1 + TS2)

    - TS1= 1, TS2 = 1

    20K = 1 / (tq(3 + 1 + 1)

    20K * 5 = 1 / tq

    100K = 1 / ((BRP + 1) * tPCLK)

    - tPCLK = APB1 = 1/36MHz = 27ns

    1 / 100K = (BRP + 1) * 27ns

    10us / 27ns = BRP + 1

    BRP = 360 - 1

    BRP = 359

    is right calculation?