Skip to main content
Associate III
Jun 17, 2026 11:11 AM UTC
Solved

Can any STM32 microcontroller directly interface with DDR memory such as DDR2/DDR3/DDR4?

We are designing an STM32-based SOM and want to know whether STM32H7 controllers support DDR memory, or if DDR support is available only in STM32MP series. Please suggest compatible STM32 controllers and reference designs for DDR interfacing.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jun 17, 2026 11:51 AM UTC

Hello,

If you mean by the DDR interface in the STM32MPxx series, that’s not available on any STM32 MCUs. It’s only available on STM32 MPUs.

So the answer is no.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

3 replies

Andrew Neil
Super User
Jun 17, 2026 11:25 AM UTC

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
unsigned_char_array
Lead III
Jun 17, 2026 11:27 AM UTC

Not PC DDR.
But some STM32 MCUs support external RAM with quad/octo/dual quad spi. Some quad/octo/dual quad spi memories support DDR mode. We use that with a H7.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jun 17, 2026 11:51 AM UTC

Hello,

If you mean by the DDR interface in the STM32MPxx series, that’s not available on any STM32 MCUs. It’s only available on STM32 MPUs.

So the answer is no.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.