Skip to main content
TARHAN SAMAH
Senior
January 9, 2018
Question

CAN İ USE PB2 AZ ANY DİO

Posted on January 09, 2018 at 10:06

HELLO because luck of pins we need to use pin PB2 AZ DİO TO READ OR WRİTE, 

İS İT POSSİBLE MXCUBE ACCEPTS THAT BUT DO ANY ONE HAS A İDEA BECAUSE WE ARE DESİGNİNG A PCB WE DONT WANT TAKE A RİSK THAT İT WİLL NOT WORK ,WE COULDNT TEST THAT ON ARDUİNO stm103c8 cart 

THANKS 

    This topic has been closed for replies.

    2 replies

    Chris1
    Associate II
    January 11, 2018
    Posted on January 11, 2018 at 04:13

    PB2 can be used as a general-purpose input or output in your application (assumed using an STM32F103). 

    However, if you plan to use the embedded boot loader, you should provide a means to pull the pin low (PB2 is also BOOT1) to allow reprogramming the flash memory via USART or USB.

    TARHAN SAMAH
    Senior
    January 19, 2018
    Posted on January 19, 2018 at 12:28

    thank you very much copied