Skip to main content
Visitor
Jun 30, 2026 3:03 PM UTC
Solved

Can a USB PD DRP port be set as Sink by default for USB OTG compatibility?

I am attempting to use X-Nucleo-DRP1M1 + Nucleo-G071RB boards as data communication dock for with following behavior :

- The dock is a sink by default and UFP, so that a non PD capable mobile device can connect and communicate with a USB peripheral using the USB OTG feature (even though the mobile device isnt being charged)

- if a PD capable mobile device is connected, the dock can send a role swap requests so the mobile device is charged and connected to a usb peripheral.

 

The charging voltage is 5V.

 

It would be preferable if this behavior occurred reliably even in the case of a power cycling while remaining connected, and after repeated disconnects + reconnects.

 

I attempted to use a CubeMX project following this guide (https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Dual_Role), setting the dock’s USB-C port as default Sink and enabled USB some connectivity features to enable connection to a peripheral.

 

I do not think the behavior i seek should require use of the Toggle feature, yet the RTOS enters an error state and freezes if it not activated, so i continue with the Toggle feature enabled.

 

With the toggle feature enabled, the following has been observed :

- a non-PD mobile device linked to the dock with a USB-C cable seems to often connect as an UFP sink, wich does not allow connection to a peripheral. Manually Resetting the board seems to activate the non-PD mobile device’s USB OTG feature, allowing connection to a USB Peripheral, but disconnecting and reconnecting the USB-C cable seems to return to the same situation described at first.

- On a PD capable device, the same has been observed, but the role swaps (data and/or power) occur correctly and is able to connect to a usb peripheral with the same USB-C cable without issue.

 

Is there any way to make the USB type C port a sink by default without risk of the port becoming a source, so as to insure a non-PD mobile device can connect to a peripheral with its USB OTG feature?

 

(also, i’ll note the following : the libraries and source files provided by STM32CubeMX seem to rely heavily on macros, and a change of project setting in STM32CubeMX does not necessarily update some source files which could have been compiled with outdated macros. A full clean of the project seems necessary after new files are generated by STM32CubeMX)

FBLBest answer
ST Technical Moderator
Jul 1, 2026 10:47 AM UTC

Hi ​@Acometis_BE_elec 

Very interesting case ! Back to basics, a DRP port is, by definition, allowed to toggle between Source and Sink attachment behavior. Because of that, it cannot be considered a strictly guaranteed  Sink by default and never Source  behavior in all attach/reconnect/power-cycle conditions.

If your goal is max reliability with non-PD devices, then the most robust design is to build the port policy as deterministic Sink/UFP at attach.

Trade-off: you lose some flexibility of DRP

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

1 reply

FBLBest answer
ST Technical Moderator
Jul 1, 2026 10:47 AM UTC

Hi ​@Acometis_BE_elec 

Very interesting case ! Back to basics, a DRP port is, by definition, allowed to toggle between Source and Sink attachment behavior. Because of that, it cannot be considered a strictly guaranteed  Sink by default and never Source  behavior in all attach/reconnect/power-cycle conditions.

If your goal is max reliability with non-PD devices, then the most robust design is to build the port policy as deterministic Sink/UFP at attach.

Trade-off: you lose some flexibility of DRP

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL