Skip to main content
giambattista
Associate
June 27, 2011
Question

Calling RTC_Init

  • June 27, 2011
  • 3 replies
  • 849 views
Posted on June 27, 2011 at 12:13

Good morning everybody!

I'm evaluating ST standard device Library with STM32L discovery board.

I want to test RTC and so in my main I want to call RTC_Init and so on.

So I prepare a RTC_InitType  structure, I create a RTC_InitType pointer, than I do:

pointer = &structure

Now I call RTC_Init and I pass to it my pointer, but there is a compiler error to this instruction:

pointer = &structure

Why doesn't it work?

How can I call routines in stm32l1xx_rtc.h?

Thank you very much

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    June 28, 2011
    Posted on June 28, 2011 at 08:23

    RTC_InitTypeDef   RTC_InitStructure;

      /* Calender Configuartion */

      RTC_InitStructure.RTC_AsynchPrediv = 0x7F;

      RTC_InitStructure.RTC_SynchPrediv    =  0xFF;

      RTC_InitStructure.RTC_HourFormat = RTC_HourFormat_24;

      RTC_Init(&RTC_InitStructure);

    RTC_InitTypeDef  *ptr;

    ptr = &RTC_InitStructure;

    ptr->RTC_AsynchPrediv = 0x7F;

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    giambattista
    Associate
    June 29, 2011
    Posted on June 29, 2011 at 08:47

    Thank you for reply.

    I adopted your solutions, but my compilers return errors (IAR and Atollic).

    For example see Cattura.jpg

    If I use the second option:

    RTC_InitTypeDef  *ptr;

    ptr = &RTC_InitStructure;

    ptr->RTC_AsynchPrediv = 0x7F;

    I obtain the following errors:

    1. data definition has no type or storage class

    2. initialization from incompatible pointer type

    3. type defaulrs to 'int' in declaration of 'ptr '

    Tesla DeLorean
    Guru
    June 30, 2011
    Posted on June 30, 2011 at 05:17

    Absent a more complete view of what's going on, I'm going to assume you have some problems with #include's, #define's or some other definition for RTC_Init.

    Right click of RTC_Init, and see if the IDE provides some details about the use and definitions thereof.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..