Skip to main content
Uwe Bonnes
Chief
May 18, 2026 11:28 AM UTC
Question

C5: Is BL_COM_CFG documented?

C5  implements a way to de-activate selected boot devices. This will allow to use the system bootloader on custom board were some activity on pins used by the bootloader but not used for the bootloader would inhibit use of the bootloader. This feature has been requested before and is very welcome.

However neither in RM0522 nor in AN2606 I find the explanation for the fifferent bits. Did I miss something?

4 replies

mƎALLEm
ST Technical Moderator
May 18, 2026 11:54 AM UTC

Hello,

Do you mean the details of these bits?

mALLEm_0-1779105212541.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Uwe Bonnes
Chief
May 18, 2026 12:04 PM UTC

Yes.
The table tells "Note: For assignment of interfaces to register bits, see the bootloader documentation."
I did not find a bootloader documentation explaining the bits.

mƎALLEm
ST Technical Moderator
May 18, 2026 12:44 PM UTC

Question raised internally over this internal ticket CDM0062722.

I'll get back to you as soon as I have a feedback.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
May 18, 2026 1:08 PM UTC

@Uwe Bonnes 

Thank you for accepting the post as solution but I prefer to unmark it until I provide an answer.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.