Skip to main content
developer2
Senior
November 12, 2013
Question

c write into asm

  • November 12, 2013
  • 2 replies
  • 705 views
Posted on November 12, 2013 at 22:41

Hi All,

please somebody help me to write this c code into asm:

void EXTI9_5_IRQHandler(void)

{

  /* Clear the EXTI line pending bit */

  //EXTI_ClearITPendingBit( EXTI_Line8 );

  EXTI->PR = EXTI_Line8;

  NVIC->ICER[ EXTI9_5_IRQn >> 0x05] = (uint32_t)0x01 << ( EXTI9_5_IRQn & (uint8_t)0x1F);

  uint32_t i32=ADC_BUFFER_FULL_LEN; // actual value 20001

  ADC_Buffer_ptr1=(uint8_t *)ADC_Buffer;

  do

  {

    *(ADC_Buffer_ptr1++)=*(((uint8_t *)&(GPIOF->IDR))+1); // GPIO_Pins [15:8] into Buffer

  }

  while( (i32--) > 0 );

}

compiler is unrolling ''while'' into 7 steps always and i think that if the code will be written in asm then will not be unrolled ...

Thanks for all replies,

Kind regards

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    November 12, 2013
    Posted on November 12, 2013 at 23:03

    please somebody help me to write this c code into asm:

    I've got some leaves that need raking and tyres that need changing. This should compile fairly cleanly

    void EXTI9_5_IRQHandler(void)
    {
    uint8_t *p = (uint8_t *)ADC_Buffer;
    volatile uint8_t *q = (((uint8_t *)&GPIOF->IDR) + 1);
    int i = 20000; // or do you need 20001 bytes?
    /* Clear the EXTI line pending bit */
    EXTI_ClearITPendingBit( EXTI_Line8 );
    while(i--)
    *p++ = *q;
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    developer2
    Senior
    November 12, 2013
    Posted on November 12, 2013 at 23:14

    well, it isn't unrolled,thank you very much ...