Skip to main content
jksystem247
Associate
October 9, 2013
Question

Bypass capacitors for STM32F0 series?

  • October 9, 2013
  • 2 replies
  • 943 views
Posted on October 09, 2013 at 10:43

Hi.

I am designing a test board using STM32F0 series MCU.

On the datasheet, it states I have to attach 3 bypass capacitors(2 x 0.1uF, 1 x  4.7 uF) per each VDD. 

Is it absolutely necessary?, What is the point of using two identical capacitor, when I can use a single capacitor with about 0.2uF value? so that I only have to use 2 capacitors per each VDD pin saving me the board real-estate?

Anyone have ideas??

Thank you.
    This topic has been closed for replies.

    2 replies

    cpinkstone2
    Associate II
    October 9, 2013
    Posted on October 09, 2013 at 10:53

    Hello188

    You've just misread it. It's one 0.1uF per Vdd pin (local de-coupling) and a single 4.7uF for the chip as a whole.

    jksystem247
    Associate
    October 9, 2013
    Posted on October 09, 2013 at 11:09

    Thank you so much!!