Skip to main content
ivan239955_stm1_st
Associate II
February 4, 2008
Question

build STM32 evaluation board for less than $20

Posted on February 04, 2008 at 12:35

build STM32 evaluation board for less than $20

    This topic has been closed for replies.

    15 replies

    obtronix
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:21

    ''I see that board is creating some interest This is an early prototype

    where STM32 is driving 128 Segment (Quadruplex drive) Glass through GPIOs and can also drive bigger LCDs with more segments and operating only from a CR2025 Coin cell Battery for a long period : more than 2 years

    STOne-32''

    Really, and it driving all the time for 2 years? What power modes are you using in software?

    obtronix
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:21

    ''obtronix, have you seen this ST7 application note? ''

    I was thinking maybe you can use the STM32 internal pull-up/pull-down resistors instead of external resistors to drive the LCD three voltage levels, but you can't turn both of them on at the same time (as far as I can see),.... but short two pins together and enable pull up on one and pull down on the other, that should give you VCC/2, getting GND and VCC from the two shorted pins is easy too

    hmm I'm sure I not thinking of something

    [ This message was edited by: obtronix on 27-01-2008 00:50 ]

    slawcus
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:21

    So... STM32 designers, I have a new assignment for you. STM32 with integrated 160 segment LCD controler.

    adrian3
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:21

    Quote:

    I see that board is creating some interest :) This is an early prototype

    where STM32 is driving 128 Segment (Quadruplex drive) Glass through GPIOs

    STOne-32

    Any more details on this, as it looks as if I may be doing something similar next.

    ivan239955_stm1_st
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:21

    - WIGGLER JTAG schematic is available on many websites. For example see attached picture.

    - JTAG is not mandatory for STM32 flash programing. UART flash bootloader works happily without JTAG - just set proper levels at boot0,1 pins, attach UART1 to PC