Skip to main content
November 16, 2020
Question

Bug when erasing flash STM32F412

  • November 16, 2020
  • 6 replies
  • 2312 views

Hello. Errata writes interesting things.

2.1.7 Flash sector erase issue for sectors 5 to 11

Description

Under specific conditions, flash erase issues are observed.

The involved sectors are: 5 to 11

Workaround

Do not perform sector erase on sectors 5 to 11.

Use flash mass erase to erase sectors 5 to 11.

That is, even the conditions under the bug manifests itself are unknown? In fact, this means one thing - it will be impossible to write a correct reliable bootloader. A bootloader that resists power failures. This is true?:(

This topic has been closed for replies.

6 replies

TDK
November 16, 2020

> it will be impossible to write a correct reliable bootloader. 

That would be my interpretation as well, as doing a full erase would also erase your bootloader.

I have no background on this, but I imagine the errata was written by someone who didn't entirely understand the problem and, instead of figuring out the issue, came up with the lazy solution of "don't do that" instead.

There should be a relatively compatible STM32F4 chip you could use as a replacement. I don't see similar errata other members of the family:

https://www.st.com/resource/en/errata_sheet/dm00037591-stm32f405-407xx-and-stm32f415-417xx-device-limitations-stmicroelectronics.pdf

"If you feel a post has answered your question, please click ""Accept as Solution""."
November 17, 2020

Thanks for your feedback!

I chose the chip according to many criteria (USB with > 5 EP, 2 CAN, QSPI, SDIO, 2 UART, SPI, 2 I2C, 256kB of RAM and all this in an LQFP-64 package). The determining factor was the price. Our distributors have found this chip to be the cheapest among the STM32F4. And now I understand why. The saddest thing is that ST has no plans to fix this in future revisions:(

Andreas Bolsch
Lead III
November 17, 2020

Errata sheet says that only first rev. , i.e. 'Z', is affected, whereas 'C' and '1' are not. Unfortunately the errata sheet doesn't doesn't tell when the particular revisions were introduced, but as there are already two more recent revisions not affected, it's quite likely 'Z' won't be shipped anymore by any official distributor.

November 17, 2020

Where did you read that?

I look here and see that this bug applies to all chip revisions:

https://www.st.com/resource/en/errata_sheet/dm00183231-stm32f412xexg-device-limitations-stmicroelectronics.pdf

Andreas Bolsch
Lead III
November 17, 2020

ES0305 Rev 9 as of Oct. 2020, Table 4, this issue seems to be the only one fixed from rev. 'Z' to 'C' and '1'.

November 17, 2020

Thanks!

Hope remains:)

November 17, 2020

I found it! Thanks!

I will contact our distributors and try to find out the revision of the chips.

Andreas Bolsch
Lead III
November 17, 2020

Just checked a F412-Disco board I got in 2017 or 2018: Rev. 'C' from week 32 in 2016. So 'Z' is probably *very* early.

November 17, 2020

Thanks!

I had nothing to check, and the information "Year" - "Revision" is unrealistic to find.