Skip to main content
Arnold Bischof
Associate III
November 28, 2017
Question

Bug Report cubeMX 4.23 IAR code genereator

  • November 28, 2017
  • 1 reply
  • 631 views
Posted on November 28, 2017 at 09:02

Hello

I use cubeMX 4.23 and have seen that the code generator for IAR itroduces absolute paths in the *.ewp project file in the include section and for all used library source files which are used in the project.

I have seen that this behaviour happens, if the cubeMX code Generator is configured to 'Add necessary library files as reference in the toolchain project configuration file'. 

The former cubeMX version (4.18) I used, did not had this problem.

kind regards, A.Bischof

    This topic has been closed for replies.

    1 reply

    Houda GHABRI
    ST Employee
    May 10, 2018
    Posted on May 10, 2018 at 16:25

    Bischof.Arnold

    Hi Arnold,

    it's normal behavior i.e: when

    cubeMX code Generator is configured to 'Add necessary library files as reference in the toolchain project configuration file',the

    code generated for IARuse absolute paths in the *.ewp file.

    if you want to use relative path you can select the other option ( copy all used librairies or copy only the necessary library files).

    Regards,

    Houda