Skip to main content
andreas2
Associate II
August 3, 2008
Question

Bug in TIM firmware

  • August 3, 2008
  • 2 replies
  • 611 views
Posted on August 03, 2008 at 20:51

Bug in TIM firmware

    This topic has been closed for replies.

    2 replies

    andreas2
    andreas2Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:41

    It seems there is a nasty bug in the TIM_SelectOCxM() function in FWLib v2.0.2. Apart from being horribly ugly and unreadable, the following code destroys the value of the modified CCMR register.

    Code:

    if((TIM_Channel == TIM_Channel_1) ||(TIM_Channel == TIM_Channel_3))

    {

    /* Reset the OCxM bits in the CCMRx register */

    *((vu32 *)((*(u32*)&TIMx) + CCMR_Offset + (TIM_Channel>>1))) &= CCMR_OC13M_Mask;

    /* Configure the OCxM bits in the CCMRx register */

    *((vu32 *)((*(u32*)&TIMx) + CCMR_Offset + (TIM_Channel>>1))) = TIM_OCMode;

    }

    else

    {

    /* Reset the OCxM bits in the CCMRx register */

    *((vu32 *)((*(u32*)&TIMx) + CCMR_Offset + ((u16)(TIM_Channel - 4)>> 1))) &= CCMR_OC24M_Mask;

    /* Configure the OCxM bits in the CCMRx register */

    *((vu32 *)((*(u32*)&TIMx) + CCMR_Offset + ((u16)(TIM_Channel - 4)>> 1))) = (u16)(TIM_OCMode << 8);

    }

    Simply substituting '|=' for '=' should ''fix'' it, but i'd rather see it rewritten completely to something like the following.

    Code:

    void TIM_SelectOCxM(TIM_TypeDef* TIMx, u16 TIM_Channel, u16 TIM_OCMode)

    {

    vu16* pCCMRx;

    u16 mask;

    /* Check the parameters */

    assert_param(IS_TIM_123458_PERIPH(TIMx));

    assert_param(IS_TIM_CHANNEL(TIM_Channel));

    assert_param(IS_TIM_OCM(TIM_OCMode));

    /* Disable the Channel: Reset the CCxE Bit */

    TIMx->CCER &= ~(CCER_CCE_Set << TIM_Channel);

    if ((TIM_Channel == TIM_Channel_1) ||(TIM_Channel == TIM_Channel_3))

    {

    mask = CCMR_OC13M_Mask;

    }

    else

    {

    mask = CCMR_OC24M_Mask;

    TIM_OCMode <<= 8;

    }

    if ((TIM_Channel == TIM_Channel_1) || (TIM_Channel == TIM_Channel_2))

    {

    pCCMRx = &TIMx->CCMR1;

    }

    else

    {

    pCCMRx = &TIMx->CCMR2;

    }

    /* Configure the OCxM bits in the CCMRx register */

    *pCCMRx = (*pCCMRx & mask) | TIM_OCMode;

    }

    This avoids the stupid type-punning and is probably more efficient as well.

    (Why is the library littered with things like taking the address of a peripheral pointer, casting it to a pointer-to-u32 and dereferencing it, often in order to compare it to a constant value? Is there any reason at all to do this, seems unnecessary to me?)

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:41

    Hi andreas1,

    Thanks for pointing out this bug, I will escalate to our software team and let you know accordingly later on about your interesting feed-backs. Thx.

    Cheers,

    STOne-32.