Skip to main content
James Murray
Associate III
May 1, 2018
Question

Bug in stm32f7xx_hal_pcd_ex.c / HAL_PCDEx_SetTxFiFo ?

  • May 1, 2018
  • 3 replies
  • 750 views
Posted on May 01, 2018 at 23:12

Is the code in HAL_PCDEx_SetTxFiFo() within stm32f7xx_hal_pcd_ex.c correct?

The datasheet says:

OTG device IN endpoint transmit FIFO size register

(OTG_DIEPTXFx) (x = 1..5[FS] /8[HS], where x is the

FIFO_number)

Bits 31:16 INEPTXFD: IN endpoint Tx FIFO depth

This value is in terms of 32-bit words.

Minimum value is 16

Bits 15:0 INEPTXSA: IN endpoint FIFOx transmit RAM start address

This field contains the memory start address for IN endpoint transmit FIFOx. The address

must be aligned with a 32-bit memory location.

However, HAL_PCDEx_SetTxFiFo isn't doing that (comments removed for brevity.)

HAL_StatusTypeDef HAL_PCDEx_SetTxFiFo(PCD_HandleTypeDef *hpcd, uint8_t fifo, uint16_t size)

{

  uint8_t i = 0;

  uint32_t Tx_Offset = 0;

  Tx_Offset = hpcd->Instance->GRXFSIZ;

  if(fifo == 0)

  {

    hpcd->Instance->DIEPTXF0_HNPTXFSIZ = (uint32_t)(((uint32_t)size << 16) | Tx_Offset);

  }

  else

  {

    Tx_Offset += (hpcd->Instance->DIEPTXF0_HNPTXFSIZ) >> 16;

    for (i = 0; i < (fifo - 1); i++)

    {

      Tx_Offset += (hpcd->Instance->DIEPTXF[i] >> 16);

    }

    hpcd->Instance->DIEPTXF[fifo - 1] = (uint32_t)(((uint32_t)size << 16) | Tx_Offset);

  }

  return HAL_OK;

}

i.e. the lower 16bits are addresses in bytes ; the upper 16bits are FIFO sizes in number of 32bit words.

There is no distinction in the HAL code between addresses which are in bytes and FIFO size which must be in 32bit words. The code ought to be multiplying by four for the Tx_Offset.

e.g.

  Tx_Offset = hpcd->Instance->GRXFSIZ << 2;

and

 Tx_Offset += (hpcd->Instance->DIEPTXF[i] >> 14);

I had been using Cube 1.9.0, but the same code is in 1.11.0.

If the code is correct, please educate me!

James

    This topic has been closed for replies.

    3 replies

    James Murray
    Associate III
    May 9, 2018
    Posted on May 09, 2018 at 23:23

    Any thoughts on this from ST ?

    James

    Brian Kennedy
    Associate
    June 19, 2018
    Posted on June 19, 2018 at 21:13

    Did anyone get any clarification from ST on this?  I'm wondering the same thing.

    -Brian

    waclawek.jan
    Super User
    June 19, 2018
    Posted on June 19, 2018 at 21:22

    This is a documentation problem, not problem in the library.

    https://community.st.com/0D50X00009XkZFSSA3

    JW