Skip to main content
michal.matejasko
Associate II
July 23, 2019
Question

BUG in RM0394 Rev 4, regarding timer (TIM2) synchronization.

  • July 23, 2019
  • 1 reply
  • 674 views

When trying to synchronize (cascade) timers, specifically wanting TIM1 to provide clock for the TIM2, there is a bug in the reference manual RM0394 Rev 4.

The bug is in the recipe in the section 27.3.19, page 857, called Using one timer as prescaler for another timer, point 2.:

"2. To connect the TRGO output of TIMy to TIMz, TIMz must be configured in slave mode

using ITR2 as internal trigger. You select this through the TS bits in the TIMz_SMCR

register (writing TS=010)."

Instead of using internal trigger 2 (ITR2) as stated above, the user should use internal trigger 0 (ITR0), as stated in the Table 136 on the page 867. Moreover, there is no Internal Trigger 2 option for the TIM2/TIM3.

Sincerely,

Michal Matejasko

This topic has been closed for replies.

1 reply

ST Technical Moderator
August 23, 2019

Hello @michal.matejasko​ ,

I will take a look on your report issue and come back to you soon.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks