Skip to main content
foujanet
Associate
March 25, 2015
Question

Bug IN HAL STM32L0xx ?

  • March 25, 2015
  • 2 replies
  • 1002 views
Posted on March 25, 2015 at 13:18

Hi,

I think there is a bug in the HAL layer of ST. (version 1.1.0) My code is very simple: I initialize two GPIO (PB4 and PB5) in Interrupt.

GPIO_InitTypeDef GPIO_InitStruct;
// Configure the Port
GPIO_TO_CHECK_1_CLK_ENABLE();
GPIO_TO_CHECK_2_CLK_ENABLE();
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
GPIO_InitStruct.Pin = GPIO_TO_CHECK_1_PIN;
HAL_GPIO_Init(GPIO_TO_CHECK_1_PORT, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_TO_CHECK_2_PIN;
HAL_GPIO_Init(GPIO_TO_CHECK_2_PORT, &GPIO_InitStruct);
// Enable and set Button EXTI Interrupt to the priority 0x03
NVIC_SetPriority((IRQn_Type)GPIO_TO_CHECK_1_EXTI_IRQn, 0x03);
HAL_NVIC_EnableIRQ((IRQn_Type)GPIO_TO_CHECK_1_EXTI_IRQn);
NVIC_SetPriority((IRQn_Type)GPIO_TO_CHECK_2_EXTI_IRQn, 0x03);
HAL_NVIC_EnableIRQ((IRQn_Type)GPIO_TO_CHECK_2_EXTI_IRQn);

Then I code the IRQ handler. PB4 and PB5 are on the same IRQ vector :

void EXTI4_15_IRQHandler(void)
{
if(__HAL_GPIO_EXTI_GET_IT(GPIO_TO_CHECK_2_PIN) != RESET)
{
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_TO_CHECK_2_PIN);
counter2++;
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_TO_CHECK_2_PIN);
}
if(__HAL_GPIO_EXTI_GET_IT(GPIO_TO_CHECK_1_PIN) != RESET)
{
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_TO_CHECK_1_PIN);
counter1++;
__HAL_GPIO_EXTI_CLEAR_IT(GPIO_TO_CHECK_1_PIN);
}
}

With the debugger, I check with a breakpoint if counter1++ and counter2++ are executed.

The problem is

: In function of the order of init of gpio, just one or the both interrupt work. If I initialize PB4 then PB5 : IT(PB4): NOK, IT(PB5):OK if I initialize PB5 then PB4 : IT(PB4): OK and IT(PB5): OK

The solution:

In the file stm32l0xx_gpio.c, when the SYSCFG->EXTICR register is configured, the mask to clear the interrupt line is false. All the register is cleared, instead of just the line. The code fixed is (line 258):

//Original
// temp = SYSCFG->EXTICR[position >> 2];
// temp &= ~((uint32_t)0x0F) << (4 * (position & 0x03));
// temp |= ((uint32_t)(GET_GPIO_SOURCE(GPIOx)) << (4 * (position & 0x03)));
// SYSCFG->EXTICR[position >> 2] = temp;
//bug Fixed
temp = SYSCFG->EXTICR[position >> 2];
temp &= ~(((uint32_t)0x0F) << (4 * (position & 0x03)));
temp |= ((uint32_t)(GET_GPIO_SOURCE(GPIOx)) << (4 * (position & 0x03)));
SYSCFG->EXTICR[position >> 2] = temp;

Just a parenthesis is add for the not (~) operator. @ST microelectronics: Thanks to you to tell me if it's a bug or not. If it's a bug, could you send me a bug report number to know when this bug will be fixed in the new HAL library. And if you are already a new HAL version ( I work with the version 1.1.0), please send me the latest version. #bug-hal-gpio-interrupt-stm32l0
This topic has been closed for replies.

2 replies

foujanet
foujanetAuthor
Associate
March 30, 2015
Posted on March 30, 2015 at 11:18

@ST-Microelectronics : Hi engineers of ST-Microelectronics. 

Did you check the bug of my last post? Did you check the test unit of the library?

I would like to know if (if it's a real bug) this bug is now known from ST, and it will be fix in the next release of HAL of L0.

Thanks you.

karsten2
Visitor II
April 1, 2015
Posted on April 01, 2015 at 20:12

wow, we would have been so hit on that too, thanks for tracking this down!